Standardise fluid system components to reduce project risk and improve efficiency

Benefits of standardising fluid system components in large-scale oil & gas Projects

Scott Nunnery, Strategic Account Manager, Global Construction Services

As major oil and gas construction projects continue to break ground around the world, owner-operators are always seeking new ways to control costs, ensure long-term reliability, and maximise the return on considerable investments being made.

One strategy to consider is the standardisation of high-quality parts, components, and assemblies that make up critical fluid systems throughout the project’s footprint. These systems are often responsible for enabling many important operational processes across these complexes, whether providing simple utilities or delivering potential gases. The failure of these systems due to substandard manufacturing, low-quality material selection, or improper installation practices can create major issues for the start-up, operation, and long-term productivity of the facility.

While fluid system applications and components often represent a minor percentage of the total construction project cost, the benefits of standardising the selection of valves, small bore tubing, and tube fittings from a single, reliable supplier can be significant. Here are a few reasons why:


 

It can help optimise labour and total system expenses


Today’s oil and gas new facility construction projects are, in some instances, the size of a medium-sized city, making the scope and volume of purchase decisions a major consideration for owners. One of the main opportunities to control costs is to take advantage of standardisation and repetition of applications and components wherever possible.

This practice is especially advantageous with fluid systems, as tube and tube fitting uniformity and consistency are essential for reliable fluid and sampling system operation. For example, standardisation can help offset a lack of expertise in installation, maintenance, and operation for crews, allowing them to avoid working with different systems and components from a variety of manufacturers. Once contractors learn how to reliably install one type of tube and fitting, it becomes easier to perform installations across more systems. This process can also reduce rework by adhering to more consistent installation, operation, and maintenance protocols.

While high-quality, durably manufactured components can cost more on a per-unit basis, their importance in maintaining fluid system integrity in these processing facilities makes an investment in them worthwhile. This upfront cost can more than pay for itself by reducing maintenance, repair, and operations (MRO) expenses over the life of the system, helping contribute to lower total lifetime cost of ownership.


Site Standardisation cover White Background-1




It helps keep all EPCCs on the same page


Given the importance of fluid system applications throughout oil and gas construction projects, many projects have become increasingly specialised depending on the chemical process. For this reason, it has become more common for owner-operators to work with a variety of different engineering, procurement, construction, and commissioning (EPCC) vendors depending upon the requirements of each application.

The more EPCCs that are on-site working on different critical applications, the more beneficial it can be to standardise a specific make of tube, tube fittings, or other components sitevwide. This strategy makes it simpler for owner-operators to validate proper installation, maintain all fluid equipment throughout its lifetime, and avoid incompatibility between different parts across the entirety of the complex.

Additionally, major oil and gas projects increasingly involve EPCCs from around the globe based on their specialities, each with differing levels of knowledge and expertise about fluid system components and design. Specifying one reliable supplier, ideally one with a global reach that can help coordinate supply and navigate language barriers, can help all EPCCs gain a common understanding of the performance characteristics of the materials being used. This can eliminate some complexities during the front-end engineering and design (FEED) stage and help set up the remainder of the project for success.


It ensures quality across the entire project


In addition to easier maintenance and parts compatibility across facilities, standardisation with a reliable supplier ensures one thing over all: All critical fluid systems are made up of high-quality components that perform as specified.

When specifying fluid system components for oil and gas projects of any size, it is important to remember that not all tubes, fittings, and valves are created equal. Selecting components that are designed to maintain leak-tight performance, and that are made from higher-quality alloys that better resist corrosion, can help operators minimise risk of leaks, maintenance issues, and potential safety hazards. When all fluid systems are made up of such components and materials, owner-operators can expect high performance for the lifetime of their operations.

Interested in learning more about the benefits of standardising fluid system components and assemblies across an upcoming oil and gas project? Swagelok can help. Our Global Construction services team, working jointly with our global network of authorised local sales and service centres, can help owner-operators standardise across these kinds of projects and realise greater initial and operational success.


 

 


Explore more oil and gas insights

Petrochemical_OutlineCircle_Blue2945 (1)

Optimise medium-pressure oil & gas systems with reliable compression fittings

Petrochemical_OutlineCircle_Blue2945 (1)

Maximise deepwater well performance in demanding offshore environments

Petrochemical_OutlineCircle_Blue2945 (1)

How training can eliminate risk on oil and gas platforms



Delivering Insight Onsite-2