How to choose the right pressure regulator for your application

Understand key factors that impact pressure regulator performance 


If you manage an industrial fluid system, you know that maintaining precise process conditions is often an operational imperative. Pressure represents one of your most important conditions, and maintaining desired pressure levels requires the right type of industrial pressure regulator in your system.

Your system and application have specific needs, and there are a wide variety of regulators to choose from. How can you be sure you’re selecting the right type of regulator for your application? Keep reading to learn more about specific types of regulators and key features to look for.


Application: Analytical instrumentation

What types of pressure regulators are best for sampling sensitive media?In sensitive analytical applications, you need to maintain exact target pressure stability. Achieving this requires a regulator designed for analytical precision.

Specialised single- and two-stage spring-loaded analytical and instrumentation regulators can help users trust their test results and maintain predictable process outputs by achieving consistent pressure control. These types of regulators are commonly spring-loaded and are available in both back-pressure and pressure-reducing designs. They should also be sensitive to adjustment, allowing operators to achieve the specific pressures they need with minimal effort.


Some features to look for include:


  • Fine-pitched threads on the stem of the control spring. This helps deliver precise adjustment with low torque.
  • Different sensing mechanism options for a range of pressures. Diaphragm-sensing models perform well in applications with lower outlet pressure requirements, whereas piston-sensing models have higher outlet pressure ranges for applications that demand high-pressure control.
  • Poppets designed to resist oscillation caused by system vibration
  • Large diaphragms to have accurate low-pressure control

Application: General industrial processesWhat types of pressure regulators are best for general industrial processes?

General industrial processes require highly reliable pressure control to best protect employees, equipment, and process output quality. In some cases, components in these applications must also be able to withstand challenging operational environments.

High-quality regulators designed for general industrial process use can provide reliable service. They are typically available in larger diameters than analytical instrumentation regulators as they need to be used in larger process lines. When selecting a process regulator, look for features such as:

  • Availability in dome-loaded, spring-loaded, or combination-loaded configurations to suit your specific application. Spring-loaded options can enable precise and easy adjustment, as mentioned above. Dome-loaded options, alternatively, are good for applications with a variety of flow variations and may be able to better minimise droop.
  • Internal seals composed of materials that are compatible with the chemicals and pressures used in your system
  • Regulator bodies composed of corrosion-resistant materials, such as 316L stainless steel, that can improve component longevity in harsh operating environments

Application: High-purity, high-flow

What types of pressure regulators are best for high-purity, high-flow applications?

Certain specialised applications (semiconductor processes, for example) demand high levels of process cleanliness and involve high flow rates. Specialised high-purity, high-flow regulators are a good option for consistent pressure control in these situations.

These regulators may be available in different configurations, and the right choice for you may depend on how much you need to adjust pressures versus simply maintaining a consistent set pressure. For example, manual versions with load springs that interact with pressure-sensing assemblies can be adjusted, whereas other versions may be preset to a certain pressure or dome-loaded with gas-actuated pressure-sensing assemblies that better suit other outlet pressure requirements. Look for these features when selecting a high-purity, high-flow regulator:


  • Compact designs that allow for close spacing of system components and process lines if space is limited in your high-flow systems. Gas-actuated versions can be less than half the size of conventional diaphragm-operated pressure regulators.
  • All-welded poppet designs that eliminate the seals’ exposure to atmosphere for clean operation and positive shutoff
  • Finishes and body compositions that minimise the opportunity for contaminationWhat types of pressure regulators are best for analytical instrumentation?
  • Self-centering poppets that can help minimise creep and offer leak-tight shutoff

Applications: Sampling sensitive media

When sampling certain sensitive or volatile process gases or fluids, preheating or vaporising the sample is required to help prevent condensation and maintain representatives.

In these instances, a vaporising pressure-reducing regulator can provide some operational benefits. These regulators respond to changes in operator inputs, ambient temperatures, and other operating conditions to keep systems operating consistently and reliably. Depending on your application, vaporising regulator features to seek out may include:

  • Electronic control that can override temperature settings to prevent process fluid maximum temperatures from being exceeded, stopping the regulator from overheating without stopping evaporation
  • Low internal volumes
  • The ability to accommodate sample phase changes
  • Certification for use in critical and hazardous environment, if required

Application: Gas distribution systems

What types of pressure regulators are best for gas distribution systems?

Gas distribution applications require continuous supply for operations to continue uninterrupted. Enabling automatic switching between two gas sources if one gas supply is depleted is a good way to achieve this.

Gas cylinder changeover regulators can provide this critical functionality, enabling smooth switching between gas supply sources to ensure continuous flow. This type of regulator can help reduce costly system downtime and time-intensive maintenance. Additional beneficial features to look for in instrumentation regulators may include:




  • Convoluted, non-perforated diaphragms that provide strength, longevity, and improved pressure response
  • Metal-to-metal diaphragm seals on all stages that deliver improved material compatibility and leak tightness
  • Designs that require minimal maintenance, allowing users to trust gas distribution systems to work as intended

Application: Hazardous fluid and gas storage

What types of pressure regulators are best for hazardous fluid and gas storage?In applications where hazardous fluids or gases are stored, it is critically important to best protect operators and bystanders. Specialised tank blanketing regulators can help maintain desired pressures of inert gases introduced into the tank’s vapor space to maintain safe and consistent tank pressure and prevent the escape of hazardous vapors.

When selecting a tank blanketing regulator, look for these features:

  • Fine-pitched threads on set-pressure springs to provide improved adjustability and resolution when setting or adjusting pressure
  • Sensitive diaphragm-sensing mechanisms designed for high accuracy in detecting changes in outlet pressure
  • Regulator components such as bodies, seats, poppets, and feedback tubes composed of corrosion-resistant alloys, depending on your operating environment

 


Explore more oil and gas insights

OilGas_OutlineCircle_Blue2945

Optimise medium-pressure oil & gas systems with reliable compression fittings

OilGas_OutlineCircle_Blue2945

Benefits of standardising fluid system components in large scale oil & gas projects

OilGas_OutlineCircle_Blue2945

Maximise deepwater well performance in demanding offshore environments



Delivering Insight Onsite-2